Steps to Exercise Switch

1.  Run PMI P2T-500M40G-USB.exe
2.  Connect Switch to PC's USB port
3.  Click Connect 
4.  Set Number of Steps to 1
5.  Click Enable Switching
6.  For J2 "On" Uncheck the Control box
7.  Click Set in the left Select Path area
8.  To switch to J3 "On" Check the Control box
9.  Click Set again.  

To have it automatically switch between states
1.  Set Number of Steps to more than 1
2.  Check the control boxes to choose which arm is on for each step
3.  Type in the Frequency in Hz (1 - 250)
4.  Click Set
5.  To stop the switching, click Reset (J2 On) and then click Enable Switching